Heat Is a Warning Sign

SKF, mécanicien de vocation2026-07-31

When summer temperatures rise, vehicle components are pushed to work harder—and wheel-end bearings are no exception. While bearing failure rarely happens without warning, excessive heat is often one of the earliest signs that something in the system requires attention.

Heat: An Early Indicator of Bearing Stress

A bearing operating at a higher-than-normal temperature may be experiencing increased friction caused by factors such as improper or insufficient lubrication, contamination, excessive loads, incorrect installation, or component wear. Although elevated temperatures may not result in immediate failure, prolonged exposure to excess heat can accelerate wear, degrade lubricant performance, and significantly reduce bearing service life.

What to Look For During Inspection

As part of routine maintenance, technicians should perform temperature checks across wheel ends and compare readings between similar components. Any noticeable temperature difference should be investigated further. Common warning signs include:

  • Unusual heat at the wheel end
  • Increased noise or vibration
  • Grease leakage or discoloration
  • Rough or inconsistent rotation
  • Visible seal damage or contamination

The Value of Early Detection

Identifying bearing-related problems early can minimize unplanned roadside failures, reduce vehicle downtime, lower maintenance costs, extend component service life, and maintain reliability during peak summer operating conditions. A few minutes spent checking temperatures during scheduled maintenance can help avoid hours—or even days—of disruption later.

SKF Insight: Heat Doesn't Just Come from the Weather

While high ambient temperatures can contribute to increased operating temperatures, the most significant source of heat within a bearing system is often friction. That is why SKF engineers bearings and sealing solutions to work together as a complete system. By reducing friction, protecting lubricant integrity, and keeping contaminants out, SKF solutions help maintain optimal operating conditions and support reliable vehicle performance—even when temperatures rise.

Heat is not just a symptom of summer. It is a signal. Recognizing and addressing it early can make the difference between routine maintenance and unexpected failure.