Don’t Let Summer Wear Lead to Hub Failure

SKF, un mecánico de verdad2026-08-31

Seasonal heat, long-distance driving and heavier loads can accelerate wheel-end wear. A timely inspection can help catch the warning signs before they turn into costly downtime.

Summer miles can leave a lasting mark

Summer is a demanding season for wheel-end components. Long highway journeys, higher ambient temperatures, heavier vehicle loads and extended periods of driving all increase the demands placed on hub assemblies. Yet the effects are not always immediately visible. A hub may still seem to be operating normally even as heat, contamination or lubricant degradation begins to accelerate wear inside the bearing.

As seasonal travel slows and vehicles return to regular business operations, workshops and fleet operators have a valuable opportunity to check wheel ends for developing issues. Identifying wear at this stage can help prevent an unexpected failure later, when vehicle availability matters most.

Know the early warning signs

Hub assemblies rarely fail without warning. Changes in noise, temperature, tire condition or wheel movement can all point to wear developing inside the assembly. During inspection, pay particular attention to:

1. Humming, grinding or growling noises that change with vehicle speed or cornering.

2. Excessive heat at the wheel end compared with the opposite side.

3. Uneven or unusual tire wear.

4. Vibration, play or looseness at the wheel.

5. Damaged seals, moisture, dirt or other signs of contamination.

Why hub assemblies fail

Although operating conditions vary, many hub assembly failures share the same underlying causes: excessive heat, contamination, improper installation and normal wear over time. These factors can reinforce one another. As friction increases inside the bearing, operating temperatures rise. Higher temperatures can reduce lubricant performance, which in turn accelerates wear on internal components.

Contamination can have a similarly damaging effect. When seals are compromised, water and road debris can enter the bearing environment, affecting lubrication and bearing surfaces. Installation also matters: incorrect torque, impact damage or improper handling can shorten service life even when the component itself is high quality.

Why SKF Hub Assemblies matter

A hub assembly is more than a single bearing. It is a wheel-end system in which bearings, seals and, where applicable, sensors must work together reliably under changing loads, speeds and temperatures.

SKF Hub Assemblies are engineered as a complete wheel-end solution, bringing together premium bearings, sealing technology and sensors designed to work as an integrated system. By helping protect critical components from contamination and managing friction effectively, SKF hub assemblies are designed to support reliable performance and long service life.

For workshops and fleets, that reliability can translate into fewer premature replacements, more predictable maintenance and greater vehicle uptime - especially as business activity picks up after the summer period.

A simple post-summer check can make the difference

The transition from summer travel to normal operating schedules is a practical maintenance checkpoint. Listen for changes, compare wheel-end temperatures, inspect tires and seals, and check for looseness according to the vehicle manufacturer’s procedures. When the signs point to wear, addressing the hub assembly early can help protect surrounding components and keep the vehicle moving.

For professional technicians: always follow the vehicle manufacturer’s inspection, torque