The main function of rear suspension (and the front one) is to keep the cars main body from touching the ground and maintaining the wheels on the road. Another function is to enhance the stability on turns and to make the ride more comfortable.
A suspension system works with forces going up and down. The weight of the car pulls the car towards the ground, so there is a coil that pushes the car upwards to prevent this from happening. However, there must be another system to prevent the coil push from being excessive, which is why there is a damper. The damper’s main function is to absorb and reduce the compression and rebound that the coil has.
An independent suspension is one of the most common suspension systems along with the the solid rear axle. In order to understand one system, it is important to get the knowledge of the other. For this reason, we will first talk about solid rear axles. When one wheel is pushed up on a solid rear axle, the other wheel does the opposite..A rear independent suspension system allows each wheel to be raised and lowered without affecting the other wheel, providing a better level of tracking for a car fitted with this type of system.
In an independent rear suspension system, each wheel can be raised and lowered without affecting the other, providing a better level of traction for a car fitted with such a system. Better traction is one of the main benefits. Therefore, the advantages of this type of system appear when driving on uneven roads. In addition, as the wheels raise and lower themselves, the contact surface with the road is always the same, which prolongs the tyre's life and performance.
In any case, if you think your car is malfunctioning, a good practice is to take your vehicle to a professional mechanic. It could be dangerous and risky not to do so. Many of the signs we have discussed could also be caused by other mechanical problems that do not necessarily stem from the suspension system. Therefore, a thorough check to discover the causes may be the best thing to do.
You can check the following link to see all the suspension products SKF is carefully manufacturing for you, it is our priority to continue to create high quality products to ensure the safety of our customers.
View our steering & suspension products