The wheel bearings on your car can last a lifetime or may not last very long. It all depends on several aspects that we will discuss below.
Before talking about replacing wheel bearing, let’s take a quick look at what can cause it to fail.
The main reasons that a wheel bearing fail are:
There are ways to keep your wheel bearings in good shape. Here are some recommendations to extend the service life of wheel bearings.
Mainly, the best you can do for them is having a relaxed driving style. Extreme driving will help getting your cars wheel bearing (and other mechanical parts) worn faster, so try not to drive fast through bumpy roads (for example).
Also how was the wheel bearing fitted into your car will influence a good or bad performance. If they get fitted exceeding the specified torque the bearing will very likely get damaged, therefore it will last less time.
Also, there are specific wheel bearing removal tool to unfit and fit bearings into the car. Not using them or using them incorrectly can also damage it. That’s why our recommendation is to always rely on professionals.
In order to understand the process of fitting a wheel bearing replacement into your car, we first need to know there are two main kinds of bearings, the old generation bearings, and the new gen bearings. Old ones are a bit more complicated to mount, but technology always comes in handy to solve this kind of difficulties. In this case, the new gen SKF wheel bearing kits are much easier to install on a car.
Only few have the guts to disassemble their cars and get their hands dirty working on it, also, its recommended that if you are going to do that, you should have the knowledge to do so, as there are chances of breaking something else if we do in an incorrect way putting in risk our security. So, with this said, our recommendation is that the job is done by a professional.
If the bearings are not broken into pieces, 2/3 hours will be might be enough for a professional to take out the old one and mount the new one, if they are broken down to pieces, more time will be needed.
It depends on the reasons for the car wheel bearing to be worn out. If the reason is that it was already too old, or that the car has been sitting still for a long time, then probably the other car wheel bearings will be in a very similar state and will soon break down. In this case it would be good to make a full change.
If for example, you were driving the road and passed fast a big pothole, probably only that wheel bearing will be affected, so no need to change it in pairs. Normally, the professional who will make the change will be able to identify if there is any need to change other bearings.