Prioritizing sustainability: SKF vehicle aftermarket's mission to reduce lifecycle emissions

News2023-06-06

We are committed to extending the physical lifespan of the existing vehicle parc with our parts and services.

Repairing, reusing, and recycling instead of buying new goods holds significant importance, particularly in the automotive industry. At SKF, we fully recognize the necessary impact these practices have on the environment. For us, sustainability in the independent automotive aftermarket revolves around the overarching goal of reducing lifecycle emissions. Through our vehicle aftermarket division, SKF aims to extend the physical lifespan of existing vehicles. We understand more than ever that the initial emissions associated with manufacturing new vehicles are undeniably high. As highlighted by Philipp Herlein, SKF Vehicle Aftermarket Business Director, in a recent interview, The initial emissions of producing a new vehicle are evidently high, so it’s critical for us to maintain existing passenger cars”.

The emergence of alternative fuel vehicles, such as hybrids and electric cars, shows that the industry is progressing to combat the threat of climate change. SKFs range of products for cars, trucks and two-wheelers are being developed to enable less friction and a safe world of mobility SKF is supporting the electric vehicle revolution with full focus on all OEM development in the EV segment. And from an end-to-end environmental perspective, at SKF we need to maintain the existing fleets out there at their best condition and therefore help the overall emission balance, explained Philipp.

According to the European Environment Agency , road transport accounts for the largest share of total transport emissions - 77% in 2020 in the European Union. Moreover, individual mobility by car has the largest impact and accounts for about 40% of greenhouse gas emissions from transport. So, for an individual car owner looking for a new alternative, the best solution might be to keep their existing vehicle, maintain it properly and keep it in its best fuel-efficient condition.

Transportation is a major source of greenhouse gas emissions and today symbolizes for about 17% of these emissions. Heavy trucks represent a large portion of this. In North America, SKF was recently involved in a customer case that operates a large fleet of vocational trucks. This means that it operates in the heavy dirt and waste management sectors The SKF team decided to do a live test of SKFs seals, which are specifically designed for vocational and heavy dirt segments applications. The outcomes surpassed all expectations This real-life scenario serves as a compelling example of how SKF's products make a tangible difference. By enabling commercial vehicles to endure extended usage, SKF contributes to a more sustainable and resource-efficient society. Through innovation and dedication, SKF continues to develop solutions that enhance the longevity of vehicles, benefiting both businesses and the environment.